Technical FAQs

Ask a Question

Can you get the Visi-blade construction on 1, 2, and 3 pole molded case breakers?

You can get the Visi-blade contruction on 1 or 2 or 3 pole breakers, unit mount and I-Line. Types FA, FH, KA, KH, LA, LH, MA, MH and Mag-gard breakers with these suffixes only. Add suffix ``V`` to the catalog number.

CTA-ID : 2016261
Was this helpful?
What can we do to improve the information ?