Technical FAQs

Ask a Question

Does the new `LDB` wireway match up to the old `LD` wireway?<br />

An adapter is required to connect the old LD wireway to the new LDB wireway. See digest 173 page 11-2 for part numbers.





CTA-ID : 2016254
Was this helpful?
What can we do to improve the information ?