Technical FAQs

Ask a Question

What is the voltage range on the ATV28 460 volt unit?

The range is 400vac -15% and 460vac +10%


CTA-ID : 2015826
Was this helpful?
What can we do to improve the information ?