Technical FAQs

Ask a Question

What Class motor overload protection does the ATV58 drive has?

The ItH current setting is used for the motor thermal protection.
Adjust ItH to the nominal current which appears on the motor nameplate.
This provides Class 20 motor overload protection.

CTA-ID : 2015784
Was this helpful?
What can we do to improve the information ?