Technical FAQs

Ask a Question

Are enclosed Altivar 66 drives available in NEMA type 12 enclosures?

Yes, they are available in NEMA 1 and NEMA 12 enclosure.


CTA-ID : 2016662
Was this helpful?
What can we do to improve the information ?