Technical FAQs

Ask a Question

Have there been any changes to the MHC53VS since 1990 - 1996?<br /><br />

There was a change in 1996 or 1997 where they modified the lip and made some mounting changes. The trim is still used as the replacement for 400A series E-1 panels.

Revised 3/22/04

CTA-ID : 2016659
Was this helpful?
What can we do to improve the information ?