Technical FAQs

Ask a Question

Does Square D offer a Class 8903 Night-Master with the Type LO or LXO electrically held or mechancially held contactor?

No, the Night-Master is available with the Type S contactors only.


CTA-ID : 2016405
Was this helpful?
What can we do to improve the information ?