Technical FAQs

Ask a Question

Is a 400 amp NQOM type interior available?

There are no 400amp NQOM interiors. There are a few interiors manufactured for specific OEM customers that are above 400 amp, but there is no standard NQOM above 225 amp.

Revised 3/9/04

CTA-ID : 10714
Was this helpful?
What can we do to improve the information ?