Technical FAQs

Ask a Question

What is the replacement gate driver board for the ATV56D54N4U?

Both the gate driver board and the main control board must be changed together. The original gate driver board for this size ATV56 drive is not available.
If this board needs to be replaced, the VX5A66107 gate driver board used with the Altivar 66 can be used along with VX4A66CK1 control kit. This will convert the drive into an ATV66 drive.
It may be good to consider having the drive repaired by SquareD repair depot.

CTA-ID : 2016452
Was this helpful?
What can we do to improve the information ?