Technical FAQs

Ask a Question

Are the F-Line contactors supplied with a coil as standard?

The F-Line contactors are supplied with a coil as standard if the coil voltage code is added to the catalog number. For example, to order an LC1F115 contactor with a 120Vac coil, order an LC1F115G7. To receive this contactor without the coil, order an LC1F115.

CTA-ID : 2016252
Was this helpful?
What can we do to improve the information ?