Technical FAQs

Ask a Question

What is the part number to use to cover the unused terminals on the comb bus bar MG10285<br />

Use catalog number 60488 Tooth caps. Comes in a bag of 20. UL Recognized

CTA-ID : 2016052
Was this helpful?
What can we do to improve the information ?