Technical FAQs

Ask a Question

Does the 9001TR36 have maintained contacts <br />

No it is a momentary device

9001TR36 is a momentary operator only, contacts are not included If maintained contacts are required use a 9001 K85 Alternate Actiion module.


CTA-ID : 2016049
Was this helpful?
What can we do to improve the information ?