Technical FAQs

Ask a Question

What is required to mount a NQOD442L225CUNL interior into an MH41 box with MHC41S(or F) cover?

Remove the 3`` rail and deadfront extensions. Then install the 6`` extensions:

(2) 80110-288-02 rail extensions
(4) 21590-17081 screws
(1) 80110-291-01 deadfront extension

Add components to the mains end of interior.

Revised 3/22/04




CTA-ID : 2016649
Was this helpful?
What can we do to improve the information ?