Technical FAQs

Ask a Question

What is the maximum distance of motor lead lengths that can be used with a KLC output filter?

In specific applications, the KLC has peformed with cable runs of up to 3,000 feet (individual results may vary).
This does not include consideration for voltage drop.
Typical applications are between 200 and 1000 feet.


CTA-ID : 2016620
Was this helpful?
What can we do to improve the information ?