Technical FAQs

Ask a Question

What are the special features of the PQ3606GRIPX3 plug-in unit?

The IPX3 gives it a X3 moisture rating per IEC 529. R means it has Class R fuse clip rejection feature.


CTA-ID : 2016434
Was this helpful?
What can we do to improve the information ?