Technical FAQs

Ask a Question

What are the dimensions and weight for ATV58HD16N4XZU, ATV58HD12N4XZU, ATV58HD12M2XZU and ATV58HU90M2XZU?

Width = 9.06 inches (230 mm)
Height = 12.80 inches (325 mm)
Depth = 8.27 inches (210 mm)
The weight is 26 lbs (11.9 kg)


CTA-ID : 2015942
Was this helpful?
What can we do to improve the information ?