Technical FAQs

Ask a Question

What are the replacement load side lugs for a PTQ3680G(H or V)?

The single barrel lug is 155470,
The double barrel is 25085-348-00
The 1/2`` Keps nut part number is 23427-028-00 (torque to 35-40 ft-lbs)


CTA-ID : 2016606
Was this helpful?
What can we do to improve the information ?