Technical FAQs

Ask a Question

What is the wire size range of the lugs on the PTQ3680G(H or V) plug-in unit?

It will accept (3) 1/0-600kcmil wires per phase and neutral and
(2) 1/0-600kcmil wires for the ground lug.


CTA-ID : 2016607
Was this helpful?
What can we do to improve the information ?