Technical FAQs

Ask a Question

What is the enclosure rating for XY2CE cable pull switches?

Meets Nema Type 1,4, and 12.
IP65 Conforming to IEC529, IP657 conforming to NF C 20-010 (IP667 with booted push button.


CTA-ID : 2016245
Was this helpful?
What can we do to improve the information ?