Technical FAQs

Ask a Question

What is the difference between the LJB45BKM and the LJB45B?

The LJB45B is a 5` foot L-shaped barrier with hardware. The LJB45BKM contains (5) straight 5` barriers that are designed to be used with the barrier bracket.

CTA-ID : 2016026
Was this helpful?
What can we do to improve the information ?