Technical FAQs

Ask a Question

Is a push button, pilot light or selector switch available factory installed in the cover of a NEMA 1, 3R, (4-4X-5) stainless steel or 12 heavy duty safety switch?

Issue:
Is a push button, pilot light or selector switch available factory installed in the cover of a NEMA 1, 3R, (4-4X-5) stainless steel or 12 heavy duty safety switch?
Product Line:
30mm Push Buttons
Environment:
9001 K/SK/KX
Cause:
Need clarification on how to order operator with flush plate.                       
Resolution:                                                                 
These are available on heavy duty UNFUSED safety switches and on all double throw switches. Wiring to contact blocks is not available. Customer must furnish catalog number of push button, pilot light or selector switch desired. This is UL listed. Add suffix PB to the switch catalog number and order by description. See Supplemental Digest for price adder.
 
Was this helpful?
What can we do to improve the information ?