Technical FAQs

Ask a Question

Does the enclosed Altistart 48 include a shorting contactor?

Yes, a shorting contactor is standard on all enclosed Altistart 48 soft starters.
The soft starter itself does not have an internal set of shorting contacts. The shorting contactor is separate from the soft starter and is installed in the enclosure with enclosed units.

CTA-ID : 2016393
Was this helpful?
What can we do to improve the information ?