Technical FAQs

Ask a Question

What is the size of the transition section for 5/15kV N3R outdoor HVL/cc to Masterclad metalclad switchgear?

Issue:
What is the size of the transition section for 5/15kV N3R outdoor HVL/cc to Masterclad metalclad switchgear?

Product Line:
MasterClad.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The section is 22`` wide plus a 3`` collar. Approximately 60`` deep and 90`` high. This is for rear alignment.


CTA-ID : 2016399
Was this helpful?
What can we do to improve the information ?