Technical FAQs

Ask a Question

Does the Model III substation with an HVL/cc switch on the primary ship in one piece? Does it have lifting eyes? Where are the eyes located?

The Model III substation ships in two pieces, the HVL/cc switch and the transformer section. The HVL/cc switch has removable lifting eyes on the top. The transformer has eyes in the base channels. It can be lifted by a crane with clevis pins, slings and a spreader bar.

CTA-ID : 2016398
Was this helpful?
What can we do to improve the information ?