Technical FAQs

Ask a Question

Can the 9013 pressure switches be used on an oil medium?

It will work fine on oil if the oil doesn`t react with the diaphragm causing it to fail prematurely. Confirm the compatibility of the diaphram material with the end user. The end user can obtain that information from their oil supplier. Also, is the oil flammable? If the diaphragm should leak, could it start a fire? These are issues that fall within the responsibility of the user.

CTA-ID : 2015339
Was this helpful?
What can we do to improve the information ?