Technical FAQs

Ask a Question

Customer has a 17 inch tank and need to cut the cord on a float switch. Wants a 9038JG1 but wants to cut the rod length down from 17 inches to 12 inches. Can he do this?

SQD does not have a recommended procedure for cutting the rod. Customer may do this at his own risk. Should he attempt to alter the length of the rods, removing stops or drilled and tapped portions of the rods could seriously affect the operation of the switch.


CTA-ID : 2011886
Was this helpful?
What can we do to improve the information ?