Technical FAQs

Ask a Question

What is the part number for the fan in the Size 7 Altivar 66 drive such as ATV66C23N41U, ATV66C28N41U or ATV66C31N41U?<br />

The Heatsink fan (larger fan on bottom of unit) part # for Design A is VZ3V666. There are two of these kits in each drive.
The stirring fan part # is VZ3V669. There are three of these kits in each drive.

CTA-ID : 2016005
Was this helpful?
What can we do to improve the information ?