Technical FAQs

Ask a Question

Which ATV58 Econoflex units include an internally mounted line reactor as standard feature?

Factory mounted line reactors within enclosure are included on 30-100hp @ 460v and optional on 1-25 hp.

For the 208/230v units they are included on 15-50 hp and optional on 1-10hp.

The miscellaneous option is Mod A09 when ordering.


CTA-ID : 2015999
Was this helpful?
What can we do to improve the information ?