Technical FAQs

Ask a Question

Is the included line reactor for the Econoflex unit mounted internally or externally?

When a line reactor is included with an Econoflex drive, it is mounted internally.
This is also true of the ATV58 M enclosed drives.

Externally supplied line reactors may be added if needed. This would not be internally mounted.

CTA-ID : 2015998
Was this helpful?
What can we do to improve the information ?