Technical FAQs

Ask a Question

What is the operational ambient temperature range on the Altivar ATV58?

Storage: -25 to +65 C (-13 to +149 F)
Drive controllers ATV58HU09M2 , U18M2 , U29M2 , U41M2 &  U72M2 and ATV58HU18N4 , U29N4, U41N4 , U54N4 , U72N4 &  U90N4:
  -10 to +50 C (+14 to 122 F) without derating
  -10 to +60 C (+14 to 140 F) with fan kit and derating of the current 2.2% per degree C above 50 C

ATV58HU54N4X, ATV58HU72N4X, and ATV58HU90N4X can be used at their highest VT rating in a 40 °C (104 °F) maximum ambient temperature.

Drive controllers ATV58HU90M2 , D12M2 , D16M2 , D23M2 ,  D28M2 , D33M2 , D46M2 and ATV58HD12N4 , D16N4 , D23N4 ,  D28N4 , D33N4 , D46 , D54N4 , D64N4 , D79N4
  -10 to +40 C (+14 to 104 F) without derating
  -10 to +50  C (+14 to 122 F) with fan kit and derating of the current 2.2% per degree C above 40 C

Drive controllers ATV58HC10N4X , C13N4X , C15N4X , C19N4X ,  C23N4X , C25N4X , C28N4X , C31N4X , C33N4X
   -10 to +40 C (+14 to 104 F) without derating
   -10 to +50 C (+14 to 122 F) with derating of the current 2.2% per degree C above 40 C


CTA-ID : 2010002
Was this helpful?
What can we do to improve the information ?