Technical FAQs

Ask a Question

What is the degree of protection for the ATV28?

The Altivar 28 drive is open type.
It becomes UL Type 1 (NEMA 1 enclosed) without removal of grey tape from the top of the controller and with the addition of the NEMA / UL Type 1 conduit box kit. The rating is IP20 when the grey tape is removed from the top of the controller.


CTA-ID : 2016290
Was this helpful?
What can we do to improve the information ?