Technical FAQs

Ask a Question

When replacing a Power Board in a size 6 & 7 ATV66 and the new board is not puchased as the same model number, will just replacing the rating card make the drive run correctly?

No. The correct powerboard must be used.
The rating card is only one of two components that is different in each kit.
Though the powerboards for size 6 & 7 drives are physically the same, they do have different firmware installed.
If the board is a different hp rating it is necessary to install the old rating card and program the drive for the correct rating via the software.
This programming can be done in the repair depot. Some of the field service technicians have done this EEPROM flashing.

CTA-ID : 2016223
Was this helpful?
What can we do to improve the information ?