Technical FAQs

Ask a Question

What is the hysteresis of current level for a Logic output with the Altivar 66 drive?

There appears to be a 100 ms response time between the motor current crossing the threshold and the logic output changing states.
There also appears to be a minimum hysteresis equal to about 10% of the drive`s rated current.
Due to the fixed response time, the hysteresis may appear to be larger if the motor current is changing rapidly.
This function is low priority for the ATV66 micro. It cannot be improved.

CTA-ID : 2016193
Was this helpful?
What can we do to improve the information ?