Technical FAQs

Ask a Question

Can sub-feed lugs be field installed on a NQOD Non-Linear panels?

No. Sub-feed lugs on non-linear panels are available as a factory assembled option ONLY.


Revised 4/27/04




CTA-ID : 2016394
Was this helpful?
What can we do to improve the information ?