Technical FAQs

Ask a Question

Do we offer the ATS48 in NEMA 7 ratings?


NEMA enclosure type 7 is constructed for indoor use in hazardous locations classified as Class I, Division 1, Groups A, B, C, or D as defined in NFPA 70.

SquareD does not provide Soft Starters with this type of enclosure.

CTA-ID : 2016583
Was this helpful?
What can we do to improve the information ?