Technical FAQs

Ask a Question

Do we offer the ATV58 in NEMA 7 ratings?

NEMA enclosure Type 7 is constructed for indoor use in hazardous locations classified as Class I, Division 1, Groups A, B, C, or D as defined in NFPA 70.
This is not an enclosure type built by SquareD.

CTA-ID : 2016582
Was this helpful?
What can we do to improve the information ?