Technical FAQs

Ask a Question

What is the replacement external reset mechanism for an 8536 Size 1 starter in a NEMA 12 enclosure ?

Order part number 30019-113-63 for the reset subassembly, 29206-30700 for the gasket, and 30019-121-01 for the lock nut.

CTA-ID : 2016376
Was this helpful?
What can we do to improve the information ?