Technical FAQs

Ask a Question

Does the Powerbus225 ``FA`` style plug-in units use the FA, FAL, or the FAP circuit breaker?

They utilize the FAP circuit breaker (lugs on load side only). An FAL type breaker could also be used by removing the lugs from the line side of the breaker.

CTA-ID : 2015994
Was this helpful?
What can we do to improve the information ?