Technical FAQs

Ask a Question

Do we offer the ATV58 in NEMA 3R outdoor rating?

The altivar 58 is an open type drive. It is no available as NEMA 3R enclosed as a stand alone unit.
However, the 8839 Econoflex type enclosed drives can be obtained in NEMA 3R rating as a standard drive offering for variable torque applications.
The Econoflex is an enclosed drive that includes disconnect, line circuit breaker and controls. The drive that is inside the enclosure is a FLEX58 which is made of the same componants as the ATV58 drive but is mounted differently to allow for optimum use inside the enclosure.


CTA-ID : 2016087
Was this helpful?
What can we do to improve the information ?