Technical FAQs

Ask a Question

Can an MAL breaker be backfed if it is in its own enclosure?

Yes. Unless the enclosure is specifically marked ``Line`` and ``Load``, the breaker can be fed in either direction.


CTA-ID : 2016576
Was this helpful?
What can we do to improve the information ?