Technical FAQs

Ask a Question

Can I wire an XS proximity sensor to control a Size 3 contactor?

No. The prox sensor has a 200ma output current, which is too low for a Size 3 contactor. Recommended using an interposing relay to switch that higher current.

CTA-ID : 2016565
Was this helpful?
What can we do to improve the information ?