Technical FAQs

Ask a Question

Will an XMLA pressure switch work with air or water?

These switches are compatible with hydraulic oils, Fresh water, sea water, air up to +70 degrees C. The 8th character in the part number determines which media the switch is compatible with.

CTA-ID : 2016564
Was this helpful?
What can we do to improve the information ?