Technical FAQs

Ask a Question

Is the QO2L30S rated for DC voltage?

NO, this load center is not UL for dc ratings. The QO24L70F/ S or RB are UL for dc.


CTA-ID : 2016320
Was this helpful?
What can we do to improve the information ?