Technical FAQs

Ask a Question

Is there a lug kit for the S33931 that will accept (4) 600 MCM cables per phase?<br />

No, the lugs on the S33931 accept (4) 3/0 to 500 mcm per phase. There is another kit, S33930, that will accept (4) 3/0 to 600 mcm per phase, but it requires 15 inches of mounting space instead of the 9 inches required by the S33931.





CTA-ID : 2016339
Was this helpful?
What can we do to improve the information ?