Technical FAQs

Ask a Question

What is the largest branch circuit breaker that can be used in a SC2040M200C?

Maximum Branch breaker rating

Product Line:
Combination Service Entrance Devices

Branch breakers

larger loads used with branch breakers.

The largest branch breaker that can be installed in this CSED is 100 amps Max. This is due to the single row construction of the interior and heat rise testing.

CTA-ID : 2016337
Was this helpful?
What can we do to improve the information ?