Technical FAQs

Ask a Question

Due we offer a low pressure cut off feature on the 9013 switches that will operate at 100 to 120 PSI?

No, the low pressure cut off form M4 is only available on the 9013FSG and FYG pressure switches which have a maximum cut out range of 80psi. At pressures over 80 psi, the momentary run switch is not capable of overcoming spring resistance for sustained operation.


CTA-ID : 2016161
Was this helpful?
What can we do to improve the information ?