Technical FAQs

Ask a Question

What tenant (branch) circuit breakers are used with the older style EZMT-200 amp branch device?

Issue:
Current design repair parts

Product Line:
EZM Metering Equipment

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The older style EZMT-200 amp single phase in, single phase out and three phase in, single phase out uses Q2M, Q2M-VH or Q2MH breaker, dependent upon AIR rating required. These tenant breakers are ALL obsolete and no longer available, but replaced with the newer Powerpact Q-Frame breakers.
 
The EZMT-200 amp three phase in, three phase out used QE type breakers. ALL the QE type tenant breakers are obsolete and no longer available with NO replacement.


CTA-ID : 2007089
Was this helpful?
What can we do to improve the information ?