Technical FAQs

Ask a Question

Can a single pole FAL breaker be installed in the FA060X, FA060Y, FA100Y, FA100X, FA100S, FA100F, FA100AWK, FA100A, FA100DS and FA100RB circuit breaker enclosure?

Issue:
Product design features

Product Line:
Circuit breaker enclosures

Environment:
Single pole Circuit breakers

Cause:
application

Resolution:

These enclosures are UL Listed and marked for use with a 1-pole, 2-pole or 3-pole FAL, FHL or FCL circuit breakers. This information is valid as of January 30, 2003. Devices manufactured before this date will not have the 1-pole schematic on the wiring diagram, although the 1-pole breaker will physically mount into the enclosure. This information is also valid for FA100F, FA100AWK, FA100DS, FA100RB and FA100S. 

 
Was this helpful?
What can we do to improve the information ?