Technical FAQs

Ask a Question

Can a single pole FAL breaker be applied in a FA100Y circuit breaker enclosure?

Yes, this enclosure will accept one 1-pole, 2-pole or 3-pole FAL circuit breaker. This information is also valid for FA060X, FA060Y and FA100X.

CTA-ID : 2016335
Was this helpful?
What can we do to improve the information ?