Technical FAQs

Ask a Question

Which side of the enclosure is the HVL operating handle on? Can it be mounted on the other side?

The HVL operating handle in on the left side of the enclosure and the fuse door opens to the right. The handle can not be moved to the right hand side.


CTA-ID : 2016316
Was this helpful?
What can we do to improve the information ?